请问:
需要外接压力传感器,系统只有5V电源,传感器参数15V供电,最大电流60mA,TI简单一点的方案?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
先用一个TPS60131之类的芯片输出稳定的5V电源,然后用一个3倍升压电路升到15V
Seasat,
现在已经有一个5V电源,3倍升压该选哪个电路呢?
谢谢!
Hi
只是做升压还是对5V电压三倍放大?
只是做升压,选择很多,如LM2731: http://www.ti.com/product/LM2731, 效率不错,封装也小。
http://www.ti.com/product/TPS61093
TPS61093: http://www.ti.com/lit/ds/symlink/tps61093.pdf 不启动时输入输出断开。