This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100应用问题求助

Other Parts Discussed in Thread: BQ34Z100, BQ34Z100-G1, BQ28Z610
由于电池带PACK后只有二线输出,BQ34Z100电路部分只能做在外部电路中,现在是硬件设计原理框图如下,BQ34Z100电路部分接地点为SRP,其它的单片机及负载部分接地点为SRN.1,BQ34Z100电路部分与单片机部分不共地,不知道这样会不会影响I2C通信及采样精度?
2,充电时,BQ34Z100采样电阻R30处电压为负值,放电时为正值,这样有什么影响?IC引脚最大负值电压不超过0.3V.
3,有没有同样的应用案例分享.第一次用这个IC,希望多多指教.

    • BQ34Z100的地选在SRP,可以更精确的测量电池两端的电压,保证采样的精度,采样电阻上的微小压降不会对IIC通信造成影响

  • 象我这样带PACK后不能采样到电芯二端电压,会不会影响很大,有没有必要让电池厂家从电芯处引出二根线作电芯电压采样?

  • 非常不建议这样使用,BQ34Z100-G1是一个电池端的电量计,目前的接法意味着只要电池那边保护断开,BQ34Z100-G1就会被复位,而如果充电器插入,也会认为电池在而错误的进行初始化。这样都会很大的影响电量计的精度。

  • 那就是建议做在PACK里,然后引出四条线:PAK+  PACK-   SDA   SCL是吗?象下图的接法:

  • 我也非常想知道 请及时回复 我也遇到了同样问题 谢谢

  • 思想是这样子的,不过你这个例子是BQ28Z610的,开关管在上面,一般配合BQ34Z100设计的电路,开关管在下面,那么可能不能够直接引出I2C,否则放电保护之后会有危险,需要处理一下,但是不管如何,BQ34Z100应该是直接连接到电芯那边。

x 出现错误。请重试或与管理员联系。