您好!我目前使用电荷泵TPS60403进行降压,从6.8V降压3.4V。实验结果发现在上电的瞬间(大概100ms)电流比较大,大概在30mA。由于这个产品用在DCS上卡件无法输出30mA的启动电流以至于无法工作。分析了好久感觉就是电荷泵的原因引起的。请问有什么办法可以控制电荷泵的上电电流么?怎么解决?
电路图见附件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
30mA的inrush电流,如果要减小或只能讲所有的电容都缩小一点看看。
H
在输入线路上增加一个10ohm的电阻。
chargepump电路是电容充放实现电压转换的,增加电阻或可以减低电流。 而本身电流需求很小,10ohm的电阻上压降几乎可以忽略。
Hi
输入的路径上,可以再输入电容前面。(输入电容1uF即可).