This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61251DSGR 和TPS61252DSGR有什么区别,两颗料可以替换吗?

Other Parts Discussed in Thread: TPS61251, TPS61252

TPS61251DSGR 和TPS61252DSGR有什么区别,两颗料可以替换吗?

  • Andy,

       TPS61251与TPS61252的区别如下,具体请查看附件。可替代。

    1.TPS61251 is optimized for charging bulk capacitors

    2.TPS61252 is a regular boost converter.

    3.TPS61252 current accuracy is 20% vs 10% from TPS61251

    4.Snooze Mode only available with TPS61251

     

    TPS61251 & TPS61252 differences.ppt
  • 5. Power Good function is different for both devices:

    TPS61251

    PG is set high if the feedback voltage reaches 95% of its nominal value.

    The PG comparator operates even in shut down mode when EN is set to low and/or VIN is turned off. This guaranties power good functionality until the capacitor is discharged.

    The PG output goes low when:

    Vout < 2.3 V and indicates the discharge of the capacitor.

    Vout < 2.0 V all internal circuitry is disabled. Therefore the PG open drain output becomes high resistive and    follows the voltage the pull-up resistor is connected to.

    While the output capacitors are still charged the converter can be disconnected from its supply but it will still supply a follow-on circuitry with energy needed for a secured shut down.