做汽车液压导航阀组驱动,从主控DSP28335输出3.3V以内占空比可调的PWM波,希望控制输出电流0~2.5A,进而驱动液压导航阀组,导航阀组额定电压12V ,请问有好的芯片推荐嘛?LM5026可以嘛?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你的输入源电压是多少? 将这个电压转换成为12V/0~2.5A, 定电流设计,必须要做隔离? 还是说可以直接用DC/DC?
我之前用的光耦隔离+VMOS开关管+BUCK降压电路搭接了一个电路,感觉不是太稳定,所以想看看有没有其他好的集成芯片,一步到位~输入电压是3.3VDSP28335的PWM~
Hi
如果你本身是用DSP搭的一个buck电路是可以的.
但是如果你想用模拟芯片来做,或可以用TPS61088: http://www.ti.com.cn/product/cn/TPS61088/toolssoftware
这款芯片通常是定电压设计,如果作为定电流设计,建议增加一个运放将其输出给到FB用以提高效率,同时将PWM信号滤成直流给到运放作为电流调节。
是的,你可以利用Ti的Webench软件进行参考设计http://www.ti.com.cn/product/cn/TPS61088/description谢谢