芯片资料上说UCC27210是UCC27200的升级版本,我见TI的UCC27200数据手册上有典型应用电路,即在UCC27200的前级有一片UCC27424芯片,我不知道UCC27424这款芯片在电路中是起什么作用的,还有是否在UCC27210的电路中也必须加上这款UCC27424芯片????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
就输入的驱动信号而言,UCC27200与UCC27424的差异在于前者非常高,需要到5.8V以上,而SN74HC74D电平输出将低于供电5V, 所以中间增加UCC27424驱动芯片,可以将驱动电平信号提高。但是如果采用UCC27201则应可以不需要增加UCC27424电路。(此电路为驱动芯片评估板)
所以在你的电路中,是否要选择UCC27424取决于你的电源芯片的PWM信号电平输出。
那您的意思是如果我采用如UC3875这样的芯片在+15V供电电压时是不需要UCC27424的,是这个意思吗???
还有UCC27210芯片的地是否一定要和主电路的地共地呢????我是否可以在驱动芯片的前级加一个光耦,起到减小输入噪音和隔离功率地和系统地的作用????
如果你的驱动信号时3875输出的驱动信号,那么信号幅度满足27200的要求,就不需要中间加27424了