Other Parts Discussed in Thread: LM5161-Q1, LM5106
我公司现在有个电动车相关的项目,需要一个降压DC-DC
输入电压12-100V,输出电压5V/1.5A,请问一下有什么IC可以推荐的,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问一下是否有直接使用BUCK降压形式的方案吗?因为现板子的空间还是比较有限的,电路可能简单一些,类似LM5161-Q1这种直接使用BUCK来实现
Hi
类似于LM5161-Q这类耐压100V左右的芯片TI是非常少的,而你的电流需求是1.5A,也很大,TI是乎没有其他类似简单的芯片可以很容易就实现。
所以我之前推荐用隔离方案来做。
或者你可以找一些半桥驱动芯片来做,例如LM5106: http://www.ti.com.cn/cn/lit/ds/symlink/lm5106.pdf
再选择一个低成本的芯片与之搭配。