This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

POE++ (TPS23754,TPS2376H)相关问题咨询啊

Other Parts Discussed in Thread: TPS23754, TPS23756, TPS23770, TPS2375, TPS23750

  

        你好大侠

最近在做POE供电设备,有几个问题想请教下

1,、TPS23754和23756工作电压不一样吗?同样的变压器,同样的负载,23754的要33V以上才能正常带载,而23756不到20v就可以,外部适配器模式!

2,、PSE的输出功率在足够大情况下,输出PD的功率是哪个决定的,比如PD设定 3 class  ,当其他情况导致大于这个功率,是PD先保护,还是PSE断电?

也就是说PSE 90W  PD25W  ,PSE输出功率是90W 还是25W的限制,PSE的输出多大的功率 由PD决定吗 ??

3、如果想获得更大的 PD的 功率?也就是非标准的供电方案,TI这有样的方案吗 30-70W

4、TPS23754和23756   30W 的反激做出来了,但是正激的反峰电压比150V都高,震荡什么的测试了都正常,加了些消峰电路,电压下来了,但是电路部件比较热损耗也高了,变压器是仿制的,反峰电压太高难道是变压器漏感太大了吗?

5,有没有不用变压器隔离的作法或方案啊 TPS23754和23756   可以改成非隔离方式的吗

 

                              期待你的解答