关于bq27510电池SOC、RM、FCC数据更新问题,在读取bq27510时,充电百分比,剩余电量,满充电容量一直没有改变是什么因素引起的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我也在用27510-G3 要读准SOC,需要用Studio进行参数配置、校准、CHEM-ID选择、循环学习。最后查看Update Status为0x02就可以了。你可以参考附件的word文档,是从论坛摘抄的。
请问,我用Studio对BQ27510-G3进行标定,已经完成循环学习,Update Status为0x02,SOC也正确,但是生成量产文件.srec文件后,导入新的芯片后,新芯片就不响应了,Studio显示写完了512,是哪里不对吗?附件有.srec文件
http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/46539.aspx你看看这个帖子
不管怎么讲,在设计一个应用的时候,都是需要先选择一个适合的ID的,然后才能够进行下一步。不过这个倒是和SOC/FCC/RM不变化无关,上面的两位不同的问题里面提高了一个,update status=02,这个代表的仅仅是Qmax和Ra table进行了更新,但是阻抗跟踪算法并没有打开,所以还需要发送命令是能IT算法,这个时候update status=06. 对于没有学习过的电池,也应该是04。
下面一个基本的阻抗跟踪算法的流程供参考。