This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050软件电流参数配置疑问



关于电流采样电阻和AOLD疑问如下:

1)数据手册:The device is designed to support a 1-mΩ to 3-mΩ sense resistor,是不是指的检测电阻值不能超出范围?

2)见图

AOLD软件设置参数最大0xFF,请问对应的是电流值是多少?条件: 1-mΩ电阻,RSNS=0。但是TableA-1表格中最大是0x0F,没有0xFF,我如何计算电流值?

  • 1. 是的,推荐的电流senser不要超过3mohm

    2. 0Xff表示的是这个栏位能填写的最大值,超过0XFF写进去会提示错误。

    Table A-1 详细列出了每个值对应的电压/检测电阻的阻值=AOLD的保护电流。

  • 还是没明白,默认值0xf4表格里面就没有啊,对应电流值是多少?怎么计算的?

  • 而且TableA-1只列出了16个对应值,软件设置可以到255个呢,这是怎么回事?到底是只能设置16个,还是能设置255个对应值?

  • 如我在另外的帖子里面的回复,高低四位对应的是延时和阈值,你对应表格查就知道了。

    另外,关于采样电阻也未必一定要是1~3mOhm.但是不同的电阻对应的你可以设置的最大硬件保护阈值范围还有步长也会不一样。理论来讲,采样电阻越大,那么ADC的采样精度会越高,但是必须保证输入不能超过ADC的输入范围,同时你能设置到你期望的硬件保护阈值。同时,电阻值大对应的也是功耗的增大。