This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq20z45 和 bq76930电池电压和温度采样精度

Other Parts Discussed in Thread: BQ76930, BQ20Z45, BQ40Z50-R1

Hi  

   请教下TI的工程师们,bq20z45  和  bq76930电池电压,温度,电流采样精度是在多少范围以内呢? 

  • 这是两个完全不同的芯片,BQ20Z45是一个集成的支持2~4S的完整电池管理方案,可以针对相应的电压,电流和温度进行校准,所以精度非常高,电压1~2mV;电流1~3mA,温度1度左右,当然会受温度范围的一点影响。不过BQ20Z45已经是比较老的产品了,现在最新的是BQ40Z50-R1。主要用于笔记本和无人机电池。

    而BQ76930是一个支持6~10S的模拟前端,本身集成了两个ADC进行电压温度和电流的测量。电压和温度是14位ADC,精度稍差,强烈建议用MCU进行二次校准,这样子精度达到5mV还是可以的。电流是16位ADC,精度依赖于后期的校准,但是比BQ20Z45或者BQ40Z50-R1要差一些,毕竟是使用在工业应用,高电压大电流的环境中,采样电阻也一般非常小。

  • 谢谢您的解释,非常感谢!