This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何判断流量计校准文件的准确性?



目前使用的是BQ27510-G3来计量电池的电量,目前遇到的情况如下:

前同事留下的配置文件同样 的电池使用时间为3.5小时,发现其电流校准的不准,便重新对电流进行校准,校准之后发现电池可以使用4个多小时,之前一直认为如果计量不准的话SOC ERROR会比较大,但是现在看来两个校准文件计算的SOC ERROR都很小,<3%,但是重新校准后的文件又的确提高了电池的使用时间,现在的问题就是如何判断流量计配置文件做的好不好?