This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1的电流采样电阻有范围要求么?



1.在datasheet里面看到的原话是 

The value of the current sense resistor should be entered into both CC Gain and CC Delta parameters in the
Data Flash Calibration section of the Evaluation Software.

但是CC Gain  范围是min 1.00E-01,max 4.00E+01,单位是mΩ,CC Delta 的范围是min 2.98E+04,max 1.19E+06单位是mΩ

这两个寄存器的参数到底是怎么算的呢?跟sense resistor的关系是怎么样的呢?

我能否用1Ω的采样电阻呢,关于电阻的参数是怎样设置呢?

2.gas guaging里面的design resistance这个参数是什么意思呢?是电池的内阻么?

  • 理论上来讲并没有特别的要求,但是针对于一般的应用来讲,肯定是在1~25mOhm之间,应用的电流越大,那么采用的电阻都要越小,如果电流很小,为了得到足够的信号,那么需要采用大电阻,但是在这种情况下,一般是需要进行倍率的配置的,相应的,芯片认为的阻抗差不多也还是在原来的范围。一般来讲,这个值是不需要手动修改的,经过校正之后,软件会自动更新进去。