我们公司一款产品想使用贵司的BQ76930 和BQ78350,但是有一些地方不大清楚,请TI的员工帮我解答;
1 客户需要按下一个按键来观看电池当前的电量,是否对应BQ78350的DISP的管脚变化,但是这些LED的电量通常是多少时间?我可以通过我的MCU去配置吗?
2 由于我们是要把BQ76930 、BQ78350和电池组作为一个部件,外面只保留一个按键开关,如果电池长期放置损耗到难以维持两个芯片工作!如何来给电池组充电?能保证BQ76930 和BQ78350极限工作的电池电压是多少,我们使用的是8节锂电池。
3 BQ78350和BQ76930是否会出现死机风险?一旦出现我们如何去复位?是否要在BQ76930加一段时间的高电平?
4 如果想使用这两个产品就一定需要使用EV2300或者EV2400?