This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050容量跳变疑问



应用:2S三元电芯,1500mAH7.2V电池组

现象描述:电池组开始测试容量读取为1655mAh,电池组在此之前已经进行过两次完整充放电过程,充电到过压保护,放电到欠压保护,用以SOC匹配。

测试:放电一次步骤为:先19A2秒后1A10秒,进行53次,容量显示为1053mah,此时一切显示正常,问题出现在第54次放电,容量直接由1053mah跳变到47mah,停止放电进行充电,充满后读取容量为700mah,电压显示正常8.3V。

疑问:为什么会出现跳变,而且是突然下降到47mah?我应该如何检查解决?谢谢

  • 因为你的负载变化很大,这种情况应该是触发到了EDV2设定点了,所以强制跳变到大约7%.这种问题首先要看你的参数设定,你采用的是固定EDV还是CEDV?你的EDV参数是如何确定的?如果你是采用的固定的EDV又不想调整电池参数,简单的可以修改EDV2 hold time到大于2S,应该可以改善。