This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60 2s电池充不上电

Other Parts Discussed in Thread: BQ40Z60

硬件是BQ40Z60-EVM-578 电芯是三洋NCR18650BF chemid是2142,设计电压3.6V,满电4.2V,放空2.5V。2串2并,设计容量6700mAh。

按照EVM手册将板子上的跳线接到2s,电池组负极接1N,1P接1S的正极,2P-4P全连通接电池组正极。

按照EVM手册将Advanced Charge Algorithm种Charge-Minimum Voltage Output设置为4350mV,将DA Configuration中的CC设置为1(2s)。做完三项电压校准。

AC电源使用稳压电源8.40V输出,使能FET_EN和CHARGER_EN,使能GAUGE。在电压低于7V的时候可以充电,但是很快电流就开始降低,但是此时SOC值只有3%,电池端电压只有7014mV。并且启用或者关闭GAUGE现象是一样的。

以下是寄存器和配置信息,状态寄存器中的MaxError那个不理解,之前在用4s电池的时候充电没有问题也就没有管它,MaxError这个值一直是100%。

请帮忙看看是否是触发了某种保护还是我的设置不对?谢谢!