This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO选型和DC/DC选型

Other Parts Discussed in Thread: TPS53353, TPS56221, LM2743, TPS54618, TPS54620

1.  input voltage 3.3V  output voltage 2.5V   output current 0.16A MAX   pls help to select LDO?

2.  input voltage 5V  output voltage 1V   output current 16A MAX   pls help to select DC/DC?

3.   input voltage 5V  output voltage 1V   output current 6A MAX   pls help to select LDO?