这边采用BQ2057W+SI6475DQ来设计锂电池充电,电源输入是12V,中间通过一个MP1482的DC/DC转成9V,输入到BQ2057W当电源输入!
现在碰到这个问题,当电压充到8.1V左右,在STAT脚上出现脉冲信号,应该就是一下充满,一下又没充满!
这边考虑是否是我DC/DC在充满的时候出现负载变化,又导致采样的电阻的电流变化,有进入充电状态?一直
死循环在这里?
不知道是否有好办法解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
建议检测一下输出的电压是多少。一般来讲,不应该在8.1V的时候就出现满充的判断,这个芯片是8.4V输出的,你的现象有点像是充饱,然后复充,因为低于8.2V就会重新充电。
检查一下芯片输出脚到电池端的电阻,电阻太大了容易出现你描述的现象。或者在充电的时候如果负载在工作也有可能出现这种情况。
这个二极管加上去会导致电池充不饱,而且不可控,因为二极管的压降也是不一致的。同时,有检测过反向漏电流多大么?因为在VCC的输入之前,是需要加一个二极管的,所以反向的漏电仅仅是给到BQ2057.这个是很小的。
你可以在输入端增加二极管,以防止电池电压反灌,就是适配器和充电IC之间增加二极管即可,这是最通常的做法。如果不喜欢这样的设计,也可以使用BQ24133一类的来做设计,使用外置的两个MOS来实现低的压降,同时保证电压不会反灌。