规格书上写
The TPS92640 and TPS92641 devices incorporate 2-Ω, 1-A internal gate drivers and supports
constant current operation up to 5 A.
最大最电流是5A,可是PMP8016 demo板上的电流是20A,是不是我理解错了规格书的内容。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你没有理解错, datasheet上的确提到以这个MOS驱动能力能支持到5A的恒流LED设计。
但是芯片实际的设计可能有出入,因素很多,例如MOS的选取,工作频率等等。