需要功能:
1、常规的过充,过放,过流;
2、带有温度保护;
3、需要电量均衡;
4、带LED指示灯,显示电量0-25%-50%-75%-100%
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
需要功能:
1、常规的过充,过放,过流;
2、带有温度保护;
3、需要电量均衡;
4、带LED指示灯,显示电量0-25%-50%-75%-100%
从你的需求来看,对于电量计的精度要求不是最高,建议采用BQ4050. 不过这个芯片是SMBUS通讯的,不过好在是从机,如果你的主机是I2C的,工作通讯是没有问题的,非常偶然的通讯不响应重读一次就可以。
汤工,我目前选择的是BQ20Z95,也是SMBUS通讯的。
是不是这个太旧了。要选择40Z50好点??
BQ20Z95确实有点太老了,BQ40Z50-R1是目前TI最新的,性能最好的1~4S的电池管理芯片了。当然没有问题。