想問一下我電源為3.3V(電池)
輸出電流為3mA
為啥峰對峰值測出來31.87mV
規格好像寫是3mV
是哪裡有問題請教各位大大
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好: 我发不了贴,我有几个问题想咨询一下,关于LM27762 芯片的
1、这颗芯片是否有升压功能???
2、PGOOD引脚具体是什么功能??
3、我现在是调试现象是,正压有输出,负压没有输出,输入为5.2V,正输出为4.99V,负输出为0,PGOOD接GND!!
1. 一般纹波测量需要示波器最小环,20MHz,如果超过正常的三角形的尖刺,认为是测试干扰,可以忽视
2. 输出纹波跟电路的电容电感占空比有关,不是固定的规格,可以计算,也可以通过webench仿真