This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210 最大带载能力

Other Parts Discussed in Thread: TPS40210

TPS40210能不能做Vin=5V Vout=20V5A?目前测试只能Vout=20V4A

  • Hi

       按照你这个条件,你应该是有额外增加驱动电路以增加芯片的驱动能实现20V/5V.

       建议你测试一下Isns,是否电流限制导致的输入电流无法提升(有可能这个时候noise偏大导致的电流保护)

       如果Isen没有保护,你需要确认一下你的电感饱和电流,按照你的参数或需要选择30A以上的功率电感。

       其次你需要注意你的输入电容,因为电流比较大,建议加大一点,否者输入有被拉低的可能,这样会加大输入电流(更易过流保护或者电感饱和),也可能欠压保护。

  • 能否帮忙查下,这颗IC最大负载能力是多少?

  • 5V输入,20V 5A输出,输入电流接近23A,而且5V供电的情况下,芯片的gate电压太低,MOS管选择的时候,需要选择5V驱动的低阻抗管子。建议使用一个小的电荷泵或者DCDC将TPS40210的供电抬高,然后再设计升压电路,升压电路的输入可以是5V。