Other Parts Discussed in Thread: BQ25895, TPS61088
TI:
我采用的方案是BQ25895锂电池充电+TPS61088升压,现有如下几个问题:
Q1:我想实现一边给电池充电,一边供系统工作,请问这样的方案可以吗?
Q2:datasheet上说这个片子是5A快充的芯片,但是输入电流最大限制为3.25A,那是不是说明快充电流不会超过输入电流限制的3.25A?
Q3:充电适配器用的ipad的(额定5.1V 2.1A),自动识别为输入电流限制2.1A,快充电流为默认值2.048A,其他寄存器值也都为默认。我在TPS61088升压后的5V接1.2A负载时基本能维持充电和放电持平,但是负载加到1.5A时不一会BQ25895就会出现过热保护,充电停止。TREG bits 也为默认的120摄氏度,请问这是什么原因导致的?
下图分别为我的电路原理图、PCB布局和1.5A过热保护时各寄存器的值,请TI工程师能够解决一下