1、TPS61260电源芯片,EN_SWICH是MCU的控制信号3.3V,在EN_SWICH输出高时,+5V-VA是马上为5V,但EN_SWICH输出低电平时,+5V-VA电压不是立刻为0,后面不加负载时是逐渐下降40秒左右还有0.1V左右。后面带负载时,一块板子是0.7v,另一块板子是0.9V。测量FB引脚也有0.1几伏的电压。电路上一共用了3颗61260芯片,其中一颗是一直使能有效,所以看不出问题。两外两颗芯片都是这现象。测试之前的老板子也有这问题。请问是为什么?
2、有关TPS61220这颗芯片,自己搭建了测试板,我输入为1.8~3.2V,输出4,5V左右,然后后面接一个TPS7A49的LDO,负载就几毫安,发现当输入为3.2V时,输出电压还比较稳,稍微有点掉,但输入为1.8V时,输出4.5V降低1.7V左右,掉的特别厉害。请问这是为什么?