This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TP71710DCK求解



你们的产品线性稳压器TPS71710DCK总是调不好,输出电压是2.25V,这是什么情况造成的呢,是不是坏了就这样啊,以前其他人有没有出现过这种情况?

  • TPS71710是一个固定1.0V输出的LDO, 只需输入输出电容,不需其他任何设定,注意输入电压不要超过最大值6.5V,

    输出2.5v肯定不正常,建议换一个新的芯片

    Pin/Package 5SC70,6SON

    Regulated Outputs(#) 1

    Iq(Typ)(mA) 0.05

    Iout(Max)(A) 0.15

    Vin(Min)(V) 2.5

    Vin(Max)(V) 6.5

    Vout(Max)(V) 1

    Vout(Min)(V) 1

    Vdo(Typ)(mV) 170

    Noise(uVrms) 30

    Approx. Price (US$) 0.36 | 1ku

    Fixed Output Options(V) 1

    Accuracy(%) 3

    Vout Adj(Max)(V) 1

    Vout Adj(Min)(V) 1

    Operating Temperature Range(C) -40 to 125,-40 to 85

    Additional Features ENABLE

    Rating Catalog

    PSRR @ 100KHz(dB) 10.35

  • 请问您输出电容使用的是电解电容还是陶瓷电容?数据手册上要求输出电容ESR小于1ohm,所以电容也不能离pin脚太远。

  • 普通的贴片电容,输出电容是1uF,换了一个新的,一上电就烧了,输出就变成2.6Vi了,他的Vin和EN都是3.26V ,是不是我们买的这个片子的质量不好啊!

  • 不能排除是来源的问题,建议您通过TI网站申请样片做下对比测试。

    www.ti.com/.../tps71710

  • Han:

        如果您的负载是在150mA以内,芯片输出电压偏离到2.5V以上,基本上可以确认是芯片质量问题。另外值得注意的是按照您的条件,需要注意一下封装选择,如果是DCK封装,芯片的最高温度可以达到25+395*(3.26-1)*0.15=158℃,所以建议您选择两外的两种封装。

     另外一个低ESR的陶瓷电容被建议,可使得输出得到纹波极低。

     您可以在以下TI网站上申请免费样片,另外TI网站上也推荐了TI的授权代理商(建议购买渠道,质量有保障)

    www.ti.com.cn/.../homepage.tsp