This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600闭环频率抖动问题



做的一个LLC拓扑的DC/DC直流源,在针对主电路做开环测试的时候,主电路上均未发生异常,但是接上控制板(控制部分和主电路部分是两块板)后,虽然其输出电压稳定,但是会出现驱动频率抖动的现象,在空载的情况下,频率会在38.2kHz~39.1kHz来回抖动,当输出功率达到200W时,驱动信号的频率在30+kHz~50+kHz来回抖动,而在闭环的情况下,主电路中的谐振电感产生噪音,发出zizizi的响声。

频率限制是33.5kHz~66kHz

目前我不清楚是因为我的频率低于了datesheet上说的限制频率出现了IC不稳定的情况还是我的参数设置出现了问题,希望各位大神能帮我看看