Other Parts Discussed in Thread: TPS55340
利用标准电路,进行TPS55340设计好后,在3V供电,空载时,输出是24V,但是加8W负载,输出变为3V多一点了。通过变大FREQ引脚的电阻更改频率,可改善到带动4W负载,输出电压为24V,但是很难实现带8W负载,24V输出,有哪些途径能实现(比如更改电阻,电感大小)让3V和22V供电,输出稳定为24V,且能带8W负载啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS55340
利用标准电路,进行TPS55340设计好后,在3V供电,空载时,输出是24V,但是加8W负载,输出变为3V多一点了。通过变大FREQ引脚的电阻更改频率,可改善到带动4W负载,输出电压为24V,但是很难实现带8W负载,24V输出,有哪些途径能实现(比如更改电阻,电感大小)让3V和22V供电,输出稳定为24V,且能带8W负载啊?
Hi
按照8.5W输出设计,效率85%,3V输入,电流就是8.5/85%/3=3.3A, 算上30%的纹波电流,输入峰值电流是3.3*(1+30%/2)=3.83A 仍小于电流保护点5.25A
所以8W输出没有问题,你需要注意如下:
1. 功率电感饱和电流选择建议大于4A
2. 输入电容需要尽量靠近电感输入端,考虑到你的输入电压太低,建议加大到40uF(2个22uF)以上
3. 频率和感量的调节只是在于电感的纹波电流,因为输出功率超过9W没有问题,可以先不调节。具体参数按照datasheet计算即可。
4. 注意功率回路尽量小。
为什么还是不行啊?把输入端的电容换位40UH以上了。附件为我的原理图和电感参数。
对了,二极管D的选型会影响吗?我用的二极管是:BYV26C-TAP VISHAY
Hi
电路图是用webench仿真的不会有问题,电感选择饱和电流4A以上,二极管选择超快恢复的肖特基二极管即可。(这些规格都可参照webench里面)
可以将layout传上来看一下。
(你选择的电感如果是15uH, 3.6A差不多,但建议再选大一点。600V/1A的二极管建议重新选,这些规格都可参照webench里面的)