我想询问一下,TPS54561芯片的最大输出功率是多大,即它在36V左右时,能输出的最大电流是多少,是5A吗,此芯片功率有这么大吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS54561这类芯片不会提及最大输出功率,而是只会提及最大输出电流, 而这款芯片是可以最大输出5A的。
故你36V输入,输出电压可以是0.8V~33V(左右),电流为5A.
这个问题这么理解。
电流能力确实可以达到5A,是指在理想情况下。但是在实际的应用中,当输出功率大的时候,损耗会同步加大,当散热条件不能满足时(芯片或外部元件过热),输出功率将不能进一步加大。而外部的散热条件取决于具体应用,半导体厂商不能预知,故无法给出允许的输出功率。