This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3429-Q1 PWM调光 噪音 输出波纹大



电路:buck-boost 升降压自适应电路, 输入电压:DC9-16V  ,输出电压16V ,恒流输出1A ,频率600KHZ,控制方式:PWM调光 频率270HZ

现象:PWM调光 模块输出1A,输出波纹平滑,波纹500mv左右,无噪音。当使用PWM改变占空比,高电平60%,输出650mA时,电感和MOS管那块有明显噪音(人耳听觉在20HZ-20KHZ),输出波纹齿状,波纹居然2.8V

修正:1、更换过电感值(22-47UH),现象无变化 2、更换过输出电容值,现象无改变,3、改变过PWM频率,从270HZ24KHZ都试过,(24KHZ时,噪音听不到,但是输出波纹突变,尖齿状),频率越低噪音越小,频率低于一定值,LED频闪。4、修改IC工作频率,由600KHZ,修改为160KHZ,现象无变化。

另外:使用模拟调光方式,则不会出现这些现象。

问题:怎么消除噪音和输出平滑的波纹??

LM3429-Q1 输出波纹大,噪音问题.doc