This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50R1 PRES引脚拉高功耗过大



想使用/PRES引脚实现MOS控制,NR=0。使用3.3V单片机IO口串联了一个100R的电阻连接到PRES引脚。

通过拉低PRES时,可以打开MOS,功耗正常。

单片机IO配置成推挽输出,强行拉高PRES,可以关闭MOS,但是PRES引脚上有10mA左右的电流。导致关机功耗超10mA 。

单片机IO配置成OD输出,拉高PRES,或者释放PRES,功耗正常,但无法正常关闭MOS。

单片机IO配置成推挽输出,增大串联电阻到1K,增大强行拉高PRES,可以关闭MOS,PRES引脚上仍有3mA左右的电流。继续增大串联电阻到100K以上,则无法关闭MOS。

请问是否有哪里配置错误,会导致芯片内部下拉PRES引脚,从而使从外部强制上拉PRES引脚会导致功耗异常?