采用bq2013管理的电池,若充电器没有连接bq2013芯片有一个done pin脚,或者应充电器充满识别错误,出现过充会怎样?如何重新复位?
如果采用充电器能识别电池充满,但没有设计与电池管理的个done pin脚连接,是否会出现bq2013电量计数器的溢出?bq2013电量计数器的溢出后,若不采用HDQ命令复位,应如何处置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用bq2013管理的电池,若充电器没有连接bq2013芯片有一个done pin脚,或者应充电器充满识别错误,出现过充会怎样?如何重新复位?
如果采用充电器能识别电池充满,但没有设计与电池管理的个done pin脚连接,是否会出现bq2013电量计数器的溢出?bq2013电量计数器的溢出后,若不采用HDQ命令复位,应如何处置?
出现过充对BQ2013在绝大多数的情况下都不会造成严重的影响,因为BQ2013的最大容量有15Ah,除非你实际的电芯容量非常接近这个极限值,但就大多数情况下我们在选择芯片的时候就会对最大容量保留一定的俗量从而避免溢出。正如之前回复你的帖子中描述的,虽然过充会增加一定的容量(非常有限),但大多数的情况下当模拟过充保护触发的时候也不会导致溢出。溢出只会发生在原始的最大容量就接近15Ah且过冲导致的那非常非常小的电量充入后刚好超过上限值,这是非常非常极端的情况。我们在选芯片的时候保留一小部分最大容量的俗量就可以完全避免这种情况发生。
我们的reset的方法分为硬件和软件两种方式
1;硬件reset;去掉VCC的同时将RBI接GND且保持15秒以上能从硬件上reset,
2;软件的reset分为两步
A:写00h到register PPFC (address = leh)
B:写 00h到 register LMD (address = 05h.)
若不使用HDQ进行reset则采用硬件复位。