This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

选型bq34Z100-g1还有几点疑问烦请解答

Other Parts Discussed in Thread: BQ34Z100-G1

您好,现初步选型bq34Z100-g1还有几点疑问烦请解答:

我们的应用场景:人体外骨骼肌医疗设备,电池使用两个13串松下18650电池组并联,标准电压:48.1V,标准容量:5.8AH。

1.  48V电池通过48V转24V再经过24V转5V输出。电量计能否接在5V后端?还是直接电池48V通过分压<22V并联?

 2.电池最大电流 Imax≈15A,电量计能否承受?

3.电池没有PACK+/PACK-是否接负载?