使用两片BQ769x0组成大于10串以上的电池组管理系统时,高位的IIC总线经过隔离芯片后,可以并接到低位的IIC总线,再接入到主控MCU上吗?
也就是说,每片BQ769x0是否有独立的片选地址,可供MCU片选,以避免占有MCU的两个IIC通信口。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用两片BQ769x0组成大于10串以上的电池组管理系统时,高位的IIC总线经过隔离芯片后,可以并接到低位的IIC总线,再接入到主控MCU上吗?
也就是说,每片BQ769x0是否有独立的片选地址,可供MCU片选,以避免占有MCU的两个IIC通信口。
TI有个参考设计,如下:
http://www.ti.com/tool/TIDA-01093?keyMatch=Bq76930&tisearch=tidesigns
High serial cell count battery (>15s) systems are becoming more and more common for industrial applications. These applications are cost sensitive and require a simple solution that includes monitoring, protection, and control or even SOC (State of Charge) information rather than only basic independent hardware protection. This design offers a platform for the complete pack side solution. All independent hardware protection features are incorporated from the bq76930 and a robust communication interface is implemented for host device to read the battery information.
谢谢!推荐的资料看了。但还是有疑问,高位的IIC可以通过关断隔离器电源实现,但低位的IIC因为是直通的。这样的话,如果只和高位的IIC通讯还是无法实现,除非低位的也加个隔离器,是这样的吗?