This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mc34063能否实现+12转-5V?

Other Parts Discussed in Thread: TPS5430, TPS5420, TPS5410, TPS5450, TPS54060A, TPS54140, TPS54040, TPS54240

想做个12V转正负5V的电路,不知道该用哪款芯片,我看Mc34063的datasheet有电压反转的电路图,但不清楚输入电压的范围该是多少。

另外,如果用TPS5430效果会不会更好,比如说纹波什么的会更小相较于MC34063,求指点,谢谢! 

  • Hi

       如果从成本的角度出发,电流不大可以选择MC34063,毕竟便宜。

       但是正如你担心的,用MC34063纹波比较大,只要增加增加了LC才会稍小。 同时如果要稍大点的输出电流,都需要外扩。

       如TPS5430这样的所有降压芯片都可以做反向输出。同时依据电流的不同,你可以选择TPS5410,TPS5420,TPS5430, TPS5450等等或其他降压芯片。

       TPS5430 TI提供的设计案例: http://www.ti.com.cn/cn/lit/an/slva257a/slva257a.pdf 采用的是内部补偿,纹波大约100mV, 这个是很大的。或者需要外部补偿会好一点。 而TI提供的TPS54060A:  只有20mV的纹波。

       所以你可以选择TPS54060A类似的TPS54040系列, 同时依据电流的不同选择TPS54040/TPS54140/TPS54240, 设计按照上述文档计算。