Other Parts Discussed in Thread: INA326, LM234, INA188
大家好,由于项目需要,想要设计一个直流电压源转电流源的电路,输出为10uA。
查阅TI的资料,发现INA326的应用电路有一个相关的设计 低电平 V-I 转换器,0V-5V 输入至 0uA-5uA 输出
但是我的负载最大为 1M欧姆,导致负载电压最大为10V,因此需要选择器件替换INA和OP,请问我该如何选择这些器件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA326, LM234, INA188
大家好,由于项目需要,想要设计一个直流电压源转电流源的电路,输出为10uA。
查阅TI的资料,发现INA326的应用电路有一个相关的设计 低电平 V-I 转换器,0V-5V 输入至 0uA-5uA 输出
但是我的负载最大为 1M欧姆,导致负载电压最大为10V,因此需要选择器件替换INA和OP,请问我该如何选择这些器件
Hi
可以选择LM234这样的电流:
http://www.ti.com.cn/cn/lit/ds/symlink/lm234.pdf
依据环境适用温度选择其不同的版本。