This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

qb25101 输入5V,输出1.9v问题??

Other Parts Discussed in Thread: BQ25101, BQ25100

电路如上图。问题:VBUS输入5V,VBAT为1V多??
1、上图为我们的原理图,是否有问题?
2、TS引脚的电阻拆掉,使TS引脚悬空,问题仍存在。
请帮忙指导一下,可能由什么原因导致的,谢谢。
  • 问题详细描述:一开始使用时,没有用锂电池。VBUS输入为5V,BQ25101的VBAT输出为4.2V。使用了一段时间后,发现好几块板的VBAT输出都是只有1.0几V了。把一块TS引脚的电阻拆掉,使TS引脚悬空,VBAT输出还是1.0几V。现在只能把锂电池插上使用了。

    1、上图的原理图,是否有问题?
    2、能否判断BQ25100芯片损坏,可能会是什么原因造成的?
    请帮忙指导一下,谢谢。

  • TS是没有接电池的NTC?另外,出现1.0几V的情况后,接上电池,还是可以正常充电的?