This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

无线charger

Other Parts Discussed in Thread: BQ500212A

 我们现在新项目有用到TI的无线充电方案,环境如下:

  1. 芯片选取上,发射端、接收端分别采取的是BQ500212A、BQ51050BRHLR;
  2. 发射端电路图如,图一;接受端电路图如,图二;
  3. 发射端线圈规格:线径:0.08*26P 感值:5.1uH  DCR:150mΩ 直径:25mm;
  4. 接受端线圈规格:    线圈(1)规格:电感30uH,外径14.3mm,线径0.4mm,线径6mm,厚度2.65mm;   线圈(2)规格:电感20uH,外径14.3mm,线径5mm,内阻460mΩ,厚度0.5mm; 

发射端电路不变动,发射端线圈规格不变;接受端线圈有两个规格供选择,现要求是充电电流为240mA,发射端和接受端线圈距离是3.6mm;

我们遇到的问题是一:线圈(1)与接收端线圈距离3.7mm左右,充电电流不稳定;

                                        线圈(2)在3.7mm左右,充电电流不稳定;

另请帮忙:

                发射端线圈电感一定,谐振电容一定;接受端基于两款线圈情况下的谐振电容如何选取,以及周围电阻达到要求电流如何选值?

                请帮忙从理论上计算出一个相对稳定的选值,谢谢!!!

x 出现错误。请重试或与管理员联系。