This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用UCC27210时候高边HO的输出电压是6V稳定的电压,LO的输出是0



如题:做一个DC-DC变换器,想先测试一下驱动芯片,LO,HO分别接入15K的占空比分别为75%和25%互补的PWM波,可是输出HO是6V的稳定电压,LO是0.

感觉芯片应该是没有烧的,驱动芯片的供电电压是12V。

  • Hi

       应该是你测试的问题,高边驱动是有一个chargepump的,这个充电电路将提供高边MOS驱动供电,如果没有正确电路可能会导致异常驱动输出。

       同时LI/HI也必须是占空比分别为75%和25%的方波。