This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,BQ24610充电发热 驱动波形异常



BQ24610做锂电池充电板 充电电压25.2V,充电电流1.5A,进入充电状态芯片发热严重起码80度以上,并且驱动波形异常。想请教一下是不是N mos选型有问题。我的板子用的Nmos和EVM板上的都是FDS8447,把EVM板上和自己买的FDS8447做了交换,一样的型号自己买的发热就比EVM板上的严重的多。FDS8447的Qg值为35-49nc。LODRV和HIDRV驱动波形如下:

都是尖波,但是手册上的波形都是方波,这个是不是因为FDS8447 Qg值过大,芯片的驱动能力不够造成的,而且发热的原因是不是也是驱动负载过大造成的。

如果是的话Qg值选多大的合适。

请TI工程师指点。