各位工程师您们好:
我想请教一下,TPS54360能输出负5V电压吗?有参考电路图吗?还是说电路和输出5V电路类似,换一下输出和地?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以做成-5V输出,参考下面设计文档:
http://www.ti.com.cn/cn/lit/an/slva317b/slva317b.pdf
TPS54360是TPS54060的3.5V输出版本,两者设计一样。
你需要将上述设计中的-12V改为设计成为-5V.
工程师您好,感谢百忙之中解答我的问题。-12V改为-5V是否更换一下电阻R1,R2的值就行了?
HI
是的,但是需要注意因为你的参数与参考设计不同,不仅仅是要变反馈电阻,其他参数也都需要计算获得。