BQ76PL455的Fault功能是不是用Fault_N引脚来通知MCU是否有Fault信息?如果有Fault信息,再通过UART读取Fault相关寄存器来获得具体的Fault信息?读完后如何reset?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的理解是对的。
FAULT_N信号可以在UART通讯出问题,或者PL455 ADC等出问题时,还是可以通知MCU在PL455发生了异常,如OV等。
BQ76PL455A-Q1有专门的squeeze功能来做断线检测,如下:
A Squeeze function in the device helps to detect open-sense wire (to the monitored cell) conditions. When the
Squeeze function turns on, it places an approximately 5-kΩ resistance across adjacent VSENSE inputs, and
creates an additional voltage drop through the approximately 100-Ω series resistors. This causes the apparent
increase in the voltage applied to the window-comparator blocks immediately above, and below, the inputs that
have the Squeeze resistor applied. Only the comparators can see the increased voltage not the AFE. This in turn
may cause the OV comparator fault to trip, even if the external sense-pin voltage measurement says otherwise,
depending on the OV threshold.