Other Parts Discussed in Thread: TPS5410, TPS5430
您好:
我按照您之前推荐的TPS5410搭建了buck-boost电路,电路图如下,其中C30.R4.C142.C95还没有焊上去,
R80用的499Ω电阻,R2用了一个可调电阻,范围是0~10k。我用直流电源供电,电压为+5.3V。
现在有以下问题:
1.上电PWM没有输出,电压没有输出,必须要把电压值微调一下才能输出。
2. 在供电过程中调节可调电阻使可调电阻小于5K,得到一个负电压值,重新上电,输出电压可以保持在断电前的电压值,最低是-15V左右;
在供电过程中增大可调电阻使其大于5K,输出可以达到-17V,但是断电后再次上电,输出只有-8V左右,不能保持在断电前的状态。只能调小可调电阻然后再次增大电阻才能再次达到-17V.