This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

超低功耗LDO选型

Other Parts Discussed in Thread: TPS783, TPS782

要求噪音小于1.5mVrms,因为主芯片使用到了ADC功能.最大不会超过20mA电流需求,持续时间不会超过200毫秒,每天唤醒2~3次,一般情况下整板待机采集消耗2uA内.深夜待机会接近50nA.

我只在选型表和在线工具看到效率等信息,但是不方便选取一个静态消耗极低的LDO.

我的输入范围就是普通的Ni-Mn电池组,默认电压3.6V.极限不超4.0V.电池组已测试可放电到1.5V自动关断.不设有充电功能,机器做好就不会拆开的.设计产品寿命要达到5年,输出电压是1.8V(最低不低于1.65V).

以前使用的是2节普通Ni-Cd电池,电压是2V,一直放电到MCU不能启动产品结束,能做到大概3年寿命.以前产品功耗比现在还大一些,现在需要更换新方案产品.希望选择一个低功耗LDO.