This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34z100问题

Other Parts Discussed in Thread: BQ34Z100

您好:

        我现在在使用贵公司的一款电量计芯片bq34z100,遇到一些问题想请教一下!

1.我看资料说bq34z100在充电学习完成过程是在充满电结束后,搁置一段时间Gas Gauging中的State中的Update Status变为05,那么我想问一下这个搁置时间需要多久?不同容量电池组搁置时间相同吗?

2.我看资料说bq34z100在放电电学习完成过程是在放电结束后,搁置一段时间Gas Gauging中的State中的Update Status变为06,那么我想问一下这个搁置时间需要多久?不同容量电池组搁置时间相同吗?

3.bq34z100如果Update State变为06,是表示学习完成了吗?学习完成以后,给电池组充电,那Update Status值会变吗?我的电量计Update State一直都是06,那以后岂不是不能再进行充电学习了吗?

4.现在我用的bq3434z100在Update state变为06以后,而且剩余电量为0,再充电,在充电的开始一段时间,电量计的剩余电量不会增长,百分比也不会上升,充大概半个小时,剩余电量开始上升,百分比上升,而且还会出现充电完成时电量计显示百分之九十五,FC未置位,这是怎么回事?

5.bq34z100什么情况下学习,学习条件是什么呢?

    • 1:对于锂电池来说,一般充满电之后放置2个小时
    • 2:对于锂电池来说,一般放电之后放置5小时
    • 3:   学习完之后再对电池充电,update status 不会变‘
    • 4:出现这种情况,有可能是一开始chem id 没有选择对,或者learning cycle没有正常进行导致的

  • 所谓的学习指的是,更新电量计芯片内的Ra table 和Qmax cell 这两个值,使之和电芯的特性匹配,需要进行一次完整的充放电电,具体参考http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/46539.aspx