您好,
关于锂电学习成功以后,我有几个问题想请教一下:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
关于锂电学习成功以后,我有几个问题想请教一下:
1,要做golden learning,首先要选择对的Chem ID。选择完Chem ID后,用EVSW设置好所有的dataflash参数,然后进行电压电流温度的校准,确认已经完成了这三个动作,才可以进行下面的步骤。然后发送命令0x41复位,等待4秒,导出SENC文件备用。
2、把电池包用0.2C电流放电到3V,然后静置5小时。
3、发送0x21命令使能IT算法,建议全程自动记录DataRAM数据(即log的数据,4秒间隔)和DataFlash数据(即自动导出GG文件,10分钟间隔)。
4、学习过程中注意观测Control Status寄存器里面的这几个标志位 RUP_DIS,VOK,QEN,在充电前确保RUP_DIS为0,VOK和QEN为1,如果没有则等待或者检测是否参数设置错误或者没发0x41和0x21命令,以及查看DataFlash里的Update Status是否为0x04。
5、满足以上条件就可以充电,电流为0.5C,电压为4.35V,一直充到电流小于设定的Taper Current值,Flags寄存器里的FC置位,即可停止充电。
6、静置2小时,观察VOK是否清零,以及Update Status是否为0x05,如果都满足,则可以开始放电,放电电流为0.2C,一直放电到实际使用设置的截止电压,然后停止放电静置5个小时。
7、观察DataFlash里的Update Status为0x06。如果还是0x05,则学习不成功。