This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于UCD9222的PMBUS烧录器连接问题的疑问

Other Parts Discussed in Thread: UCD9222, UCD7242

德仪社区的工作人员您好,我参考6678的EVM开发板设计了一块板子,DSP部分的电源模块和EVM板相同,都是采用UCD9222和UCD7242的组合。但是在购买了TI官方的USB interface adapter EVM烧录器,下载官方的Fusion Digital Power Designer后,发现软件始终显示找不到PMBUS器件,烧录器上的绿色指示灯正常,证明烧录器工作正常。烧录器的10pin插头通过杜邦线连接到PCB印制板的5芯插座上,对应信号线分别是6,7,8,9,10脚。因为实在找不出不能识别器件的原因,所以又购买6678的EVM开发板,尝试连接PMBUS后,发现同样找不到设备。电脑采用的win7 64位操作系统,想请问是否还需要安装什么驱动,或者有其他遗漏步骤,谢谢回复。