单独给一个+12V可以输出-12V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
输入上的电阻有压降,建议将R31/R32改为0欧姆或者磁珠。20欧姆的电阻即便电流只有0.3A, 输入的压降就是6V.
其次负电压的U26, 需要在-12V与输入之间增加电容(可就用这个100uF)