目前用此芯片12V转5V使用,发现在室温比较高的情况下,持续工作半小时,会突然关断,没有输出。
请大神们给看看什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,这颗芯片有高温保护,如果温度超过155, 就会自动关断,等温度降下来芯片又会正常。 请测试你在关断时的温度,并上传你的原理图以及layout,谢谢!
Hi
有点不对,输出0.4A, 芯片温升不足10℃, 我想环境温度不会超过100℃以上吧? 确认一下。