本人公司有个案子,充电部分用的是BQ25895,发现一个问题:采用适配器充电,当充电电压10V的时候是正常充电的,此时把电压下降到8V就会立即没有充电电流,必须要重新上电才能充电,这是什么情况?需要软件对寄存器进行什么配置吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本人公司有个案子,充电部分用的是BQ25895,发现一个问题:采用适配器充电,当充电电压10V的时候是正常充电的,此时把电压下降到8V就会立即没有充电电流,必须要重新上电才能充电,这是什么情况?需要软件对寄存器进行什么配置吗?
Hi
检查输入电流设置上有没有问题(同时用示波器测试一下输入电压是否是稳定的8V)?
陶工您好,输入电流设置的相关寄存器有哪些呢?我这边关于充电芯片设置:最大充电电流按照1.3A设定,启用芯片内部ICO功能,关闭芯片内部看门狗,最小系统电压3.2V,其他采用先默认设置,输入电压稳定在8V的,因为采用了直流稳压电源。