Other Parts Discussed in Thread: TPS53318
我们在使用TPS53318,纹波比较大,大约是100mV,帮忙定位下。
原理图如附件,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
DCAP模式不能直接用陶瓷电容(DCAP2模式可以),需要足够大的ESR。 如果用陶瓷电容,你需要额外引入ripple到FB来稳定。
你采用多个电容包括陶瓷电容在内作为输出电容,建议你采用datasheet的计算方式仔细确认一下。
其次layout上,注意功率环路尽量小。
从你的原理图来看,如果你的纹波注入电路(R585,C291,C292)没有接,那么你必须要接ESR较大的电容以保证反馈的精度,如电解电容。 但是这样机会导致输出纹波较大。
如果想要降低纹波,建议将输出电容换成瓷片电容,同时加入外部纹波注入电路。同时需要注意的是在设置外部纹波注入参数的时候需要保证注入纹波为10mV~15mV,具体取值可以参考数据手册.此外还要保证输出电容上的纹波以及电感上DCR产生的纹波要小于注入纹波,具体参见http://www.ti.com/analog/docs/litabsmultiplefilelist.tsp?literatureNumber=slva453&docCategoryId=1&familyId=64&keyMatch=SLVA453&tisearch=Search-EN-Everything
谢谢